2009-03-04 4:15 AM
SDIO Wide bus (4-bit) operation mode
2011-05-17 4:05 AM
Hello,
I try to write a block on a SDIO card. For that I need to set the wide bus (4-bit) operation mode (meaning data would be transferred on D[3.0]) On the datasheet of the STM32F103 it says: Wide bus (4-bit bus width) operation mode is selected or deselected using SET_BUS_WIDTH (ACMD6). The device I plugged on the SDIO doesn t support the command 6. It only supports command 52 (IO_RW_DIRECT) and command 53 (IO_RW_EXTENDED). Would anybody know how to set the SDIO bus width on 4 bits on a STM32F103? Thanks in advance.2011-05-17 4:05 AM
Quote:
On 03-03-2009 at 15:28, Anonymous wrote: Hello, I try to write a block on a SDIO card. For that I need to set the wide bus (4-bit) operation mode (meaning data would be transferred on D[3.0]) On the datasheet of the STM32F103 it says: Wide bus (4-bit bus width) operation mode is selected or deselected using SET_BUS_WIDTH (ACMD6). The device I plugged on the SDIO doesn t support the command 6. It only supports command 52 (IO_RW_DIRECT) and command 53 (IO_RW_EXTENDED). Would anybody know how to set the SDIO bus width on 4 bits on a STM32F103? Thanks in advance. SDIO_InitStructure.SDIO_BusWide = SDIO_BusWide_4b; You can follow the example: SDIO_InitTypeDef SDIO_InitStructure; SDIO_InitStructure.SDIO_ClockDiv = 0xB2; SDIO_InitStructure.SDIO_ClockEdge = SDIO_ClockEdge_Rising; SDIO_InitStructure.SDIO_MCLKBypass = SDIO_MCLKBypass_Disable; SDIO_InitStructure.SDIO_ClockPowerSave = SDIO_ClockPowerSave_Enable; SDIO_InitStructure.SDIO_BusWide = SDIO_BusWide_4b; SDIO_InitStructure.SDIO_HardwareFlowControl = SDIO_HardwareFlowControl_Enable; SDIO_Init(&SDIO_InitStructure);2011-05-17 4:05 AM
Thanks vinicius_acvasconcelos
I can see how put the SDIO in 4 bits mode. Now I ve got to find out why the data are not transferred.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.