2017-07-25 4:16 AM
HOW MANY SDIO INTERFACES ARE THEIR IN STM32F407VG ????ONLY ONE OR TWO??IF TWO ARE THEIR CAN I USE BOTH AT SAME TIME??
#stm32f407vgSolved! Go to Solution.
2017-07-26 1:52 AM
Hello !!
According to dataseet There is only one exist.
2017-07-26 1:52 AM
Hello !!
According to dataseet There is only one exist.
2017-07-26 2:49 AM
THANK YOU
I WANT TO KNOW IS THEIR ANY STM32F4 SERIES BOARD WHICH IS HAVING 2 SDIO INTERFACES????
IN STM32F7 SERIES 2 SDIO INTERFACES ARE AVAILABLE,CAN I USE BOTH INTERFACES AT SAME TIME???
FORTOUNAS.EVANGELOS
2017-07-26 3:13 AM
Please keep discussing in same thread:
https://community.st.com/0D50X00009XkXUnSAN
.No need for topic duplication.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-07-26 5:11 AM
Take a look at
. for the first question.For the second , Any peripheral can be used same time with any other peripheral;
Exceptions
pin availability for exclusive or shared use from each peripheral
Errata sheet limitations.
By definition from ST writen clear in ref manual (no company wants this kind of limitation for their products)
2017-07-26 6:16 AM
Can we also try not to type in ALL CAPS, the Internet considers this to be shouting
2017-07-26 8:58 PM
i got this information in datasheet of one of STM32F7 board
The current version supports only one SD/SDMMC/MMC4.2 card at any one time and a stack of MMC4.1 or previous.
what does it means????As we have separate pins for both interfaces ,i can communicate using 2 sdio pins with different devices at same time?????
st.mcu
FORTOUNAS.EVANGELOS
2017-07-28 4:54 PM
Hi!!
STM32F779BIT (at least) can communicate using 2 sdmmc at same time.
STM32F769NIH,,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.