2012-02-27 1:14 PM
My SDIO clock won't divide(stuck at 48mHz) and the data lines are stuck high. I've fiddle with every setting and checked the PLL several times. Can anyone spot my mistake. Thank you.
Using STM32F407 uint32_t regSDIO_CLKCR; GPIO_InitTypeDef GPIO_InitStructure; SDIO_InitTypeDef SDIO_InitStructure; /* GPIOC and GPIOD Periph clock enable */ RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOD, ENABLE ); /* Enable the SDIO APB2 Clock */ RCC_APB2PeriphClockCmd( RCC_APB2Periph_SDIO, ENABLE ); /* Configure PC.12 pin: CLK pin */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_25MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIOC->BSRRL = GPIO_Pin_12; GPIOC->BSRRH = GPIO_Pin_12; GPIOC->BSRRL = GPIO_Pin_12; GPIOC->BSRRH = GPIO_Pin_12; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_Init(GPIOC, &GPIO_InitStructure); /* Configure PD.02 CMD line */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOD, &GPIO_InitStructure); /* Configure PC.08, PC.09, PC.10, PC.11 pins: D0, D1, D2, D3 pins */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOC, GPIO_PinSource8, GPIO_AF_SDIO); GPIO_PinAFConfig(GPIOC, GPIO_PinSource9, GPIO_AF_SDIO); GPIO_PinAFConfig(GPIOC, GPIO_PinSource10, GPIO_AF_SDIO); GPIO_PinAFConfig(GPIOC, GPIO_PinSource11, GPIO_AF_SDIO); GPIO_PinAFConfig(GPIOC, GPIO_PinSource12, GPIO_AF_SDIO); GPIO_PinAFConfig(GPIOD, GPIO_PinSource2, GPIO_AF_SDIO); SDIO_InitStructure.SDIO_ClockDiv = 32;//SDIO_INIT_CLK_DIV; SDIO_InitStructure.SDIO_ClockEdge = SDIO_ClockEdge_Rising; SDIO_InitStructure.SDIO_ClockBypass = SDIO_ClockBypass_Enable; SDIO_InitStructure.SDIO_ClockPowerSave = SDIO_ClockPowerSave_Disable; SDIO_InitStructure.SDIO_BusWide = SDIO_BusWide_4b; SDIO_InitStructure.SDIO_HardwareFlowControl = SDIO_HardwareFlowControl_Disable; SDIO_Init(&SDIO_InitStructure); /*!< Set Power State to ON */ SDIO_SetPowerState(SDIO_PowerState_ON); regSDIO_CLKCR = SDIO->CLKCR; LCD_SetCursor ( 0, 0 ); sprintf( tmp, ''CLOCK %h'', regSDIO_CLKCR); LCD_write_str((unsigned char *)tmp); /*!< Enable SDIO Clock */ SDIO_ClockCmd(ENABLE); regSDIO_CLKCR = SDIO->CLKCR; LCD_SetCursor ( 0, 1 ); sprintf( tmp, ''CLOCK %h'', regSDIO_CLKCR); LCD_write_str((unsigned char *)tmp); while( 1 ) { //CMD0 Go idle. SDIO_CmdInitTypeDef SDIO_CmdInitStructure; //Structure. SDIO_CmdInitStructure.SDIO_Argument = 0x0; SDIO_CmdInitStructure.SDIO_CmdIndex = 0; SDIO_CmdInitStructure.SDIO_Response = SDIO_Response_No; SDIO_CmdInitStructure.SDIO_Wait = SDIO_Wait_No; SDIO_CmdInitStructure.SDIO_CPSM = SDIO_CPSM_Enable; SDIO_SendCommand(&SDIO_CmdInitStructure); } stm32-sdio-sdio_clk-clock-48mhz2012-02-27 5:15 PM
Try it without the SDIO clock bypass enabled, I think that defeats the divisor.
I've got this in my init and the clock divisor works:SDIO_InitStructure.SDIO_ClockBypass = SDIO_ClockBypass_Disable;2012-02-29 12:43 PM
That did it, thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.