2010-04-20 12:55 AM
Schmitt Trigger on STM32
2011-05-17 4:47 AM
There's at least 100mV uncertainty from the hysterisis alone and I doubt that the thresholds are well defined. Use an external comparator. If you are not fussy about switching levels you could use a CMOS 555 timer powered from the +3.3V STM32 supply. Just tie pins 2 and 6 together and use the output on pin 3.
2011-05-17 4:47 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.