2021-04-30 2:05 PM
Hi:
Is is possible to configure the LSM6DSOX to only capture data (Accel and Gyro) when an external trigger is given? This would be an interrupt from a host processor. The trigger may or may not be a fixed consistent frequency. I am aware of the DEN triggering where the closest sample to the external trigger is captured - can the sample be captured only when the external signal happens?
Thanks,
Joe
Follow up: Perhaps a better way to ask this: Is there a different ST Micro IMU that can be triggered to read acceleration/gyro conditions using an external signal? The LSM6DSOX does not seem to be externally triggerable.
Thanks,
Joe
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.