2018-01-08 7:08 AM
Hi, I am trying to modify the the code which is compiled from st motor control workbench. So far i have successfully run using st motor control workbench. May I ask is it possible to modify the code so that it does not need to run through the st motor control workbench which include adjusting the speed of motor just by varying the potential-meter on motor driver. If it is possible, which document do I need to refer to? Thanks
2018-01-09 1:12 AM
Hello ,
I am not responsible of ST motor control library.
I am contacting the development team about this request.
Best regards
Erwan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.