2018-06-22 5:06 PM
Hi,
Why the RTC Year is a uint8_t and value must be b/w 0 and 99? How do we map to real year? Thx
/**
* @brief RTC Date structure definition */ typedef struct { uint8_t WeekDay; /*!< Specifies the RTC Date WeekDay. This parameter can be a value of @ref RTC_WeekDay_Definitions */uint8_t Month; /*!< Specifies the RTC Date Month (in BCD format).
This parameter can be a value of @ref RTC_Month_Date_Definitions */uint8_t Date; /*!< Specifies the RTC Date.
This parameter must be a number between Min_Data = 1 and Max_Data = 31 */uint8_t Year; /*!< Specifies the RTC Date Year.
This parameter must be a number between Min_Data = 0 and Max_Data = 99 */}RTC_DateTypeDef;
Note: this post was migrated and contained many threaded conversations, some content may be missing.2018-06-25 12:39 PM
You're probably using the wrong format (BCD vs Binary), if you're reading 0x43 it is 43 minutes in BCD
BCD uses two 4-bit pairs, ie ticks from 0x09 to 0x10
You should review how you're reading the values, and the settings involved.
You're providing observation where I can't see the context.
2018-06-25 12:44 PM
Doesn't make any sense to have seconds exceed 59 either.
Name : Seconds
Details:84 'T' Default:84 'T' Decimal:84 Hex:0x54 Binary:1010100 Octal:01242018-06-25 9:51 PM
2018-06-26 12:32 AM
Thanks. This help.
On Mon, Jun 25, 2018, 9:53 PM Andrei Chichak <st-microelectronics@jiveon.com>
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.