2015-07-31 11:47 AM
I have used CubeMx to generate code for stm32f407
Set RTC internal weakupand enabled the NVICbut the RTC_WKUP_IRQHandler() never got called!code:/* RTC init function */void MX_RTC_Init(void){ RTC_TimeTypeDef sTime; RTC_DateTypeDef sDate; RTC_AlarmTypeDef sAlarm; /**Initialize RTC and set the Time and Date */ hrtc.Instance = RTC; hrtc.Init.HourFormat = RTC_HOURFORMAT_24; hrtc.Init.AsynchPrediv = 127; hrtc.Init.SynchPrediv = 255; hrtc.Init.OutPut = RTC_OUTPUT_DISABLE; hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH; hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN; HAL_RTC_Init(&hrtc); sTime.Hours = 0; sTime.Minutes = 0; sTime.Seconds = 0; sTime.SubSeconds = 0; sTime.TimeFormat = RTC_HOURFORMAT12_AM; sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE; sTime.StoreOperation = RTC_STOREOPERATION_RESET; HAL_RTC_SetTime(&hrtc, &sTime, FORMAT_BIN); sDate.WeekDay = RTC_WEEKDAY_MONDAY; sDate.Month = RTC_MONTH_JANUARY; sDate.Date = 1; sDate.Year = 0; HAL_RTC_SetDate(&hrtc, &sDate, FORMAT_BIN); /**Enable the Alarm A */ sAlarm.AlarmTime.Hours = 0; sAlarm.AlarmTime.Minutes = 0; sAlarm.AlarmTime.Seconds = 0; sAlarm.AlarmTime.SubSeconds = 0; sAlarm.AlarmTime.TimeFormat = RTC_HOURFORMAT12_AM; sAlarm.AlarmTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE; sAlarm.AlarmTime.StoreOperation = RTC_STOREOPERATION_RESET; sAlarm.AlarmMask = RTC_ALARMMASK_MINUTES; sAlarm.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_ALL; sAlarm.AlarmDateWeekDaySel = RTC_ALARMDATEWEEKDAYSEL_DATE; sAlarm.AlarmDateWeekDay = 1; sAlarm.Alarm = RTC_ALARM_A; HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, FORMAT_BIN); /**Enable the WakeUp */ HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0, RTC_WAKEUPCLOCK_CK_SPRE_16BITS);} #wakeup2015-07-31 12:44 PM
For those playing along at home..
What board are you using?What clock source are you using for the RTC?Does the RTC seem be ticking along normally otherwise?Are you setting the Alarm to some time in the future?How far in the future?2015-07-31 12:52 PM
-I am using customized board with stm32f407, I have external 32k crystal
-RTC seem be ticking along normally (when I do polling like this I see the RTC updates normally every seconds:while(1) { LCD_Display_Time(); HAL_RTCEx_PollForWakeUpTimerEvent(&hrtc,HAL_MAX_DELAY); } I did not set any alarms I just set the WakeUpTimer for every 1 secondsNevertheless, When I set the Alarm for 5 seconds, I get interrupt normallythe only problem is with WakeUp2016-04-14 8:13 AM
Hi SamTheMan,
This issue is now fixed in the new release by adding inside MX_RTC_Init(): __HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(); Before the call to: HAL_RTCEx_SetWakeUpTimer_IT();-Hannibal-
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.