2010-06-21 8:23 AM
RTC Value being lost on Sleep mode
2011-05-17 4:55 AM
The problem is likely how you are initializing the RTC when the system exits STANDBY. You need to check and clear the PWR_FLAG_SB, and you should be able to recover the time from RTC_GetCounter() and not reconfigure the RTC.
2011-05-17 4:55 AM
Sleepmode and standbymode are extremly different on the STM32!
After wakeup from standbymode, there will be a reset. RAM content is normally lost. If LSEON, LSERDY, RTCON, ... are in correct state, you have the possibility to recover the RTC. You have to reset the ''Registers synchronized flag'' and wait until it is automatically set again. This operation is slow (>30µs). You can write to the RTC registers before, but reading brings wrong values, because the shadow registers in the interface aren't initialized.2011-05-17 4:55 AM
Mine does not wake up from Standby.
I currently do it like this: ...// Peripheral Clock - This is done in the init function, but I did it again here
RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR,ENABLE); // Enable WKUP pin PWR_WakeUpPinCmd(ENABLE);// Insert a delay - I have also tried without this delay
Delay(0xFFFF); // for(; nCount != 0; nCount--);// Request to enter STANDBY mode and wake up with rising edge of WKUP pin
PWR_EnterSTANDBYMode();while(1)
{ // Infinite loop - It's OK because the system will reset anyways } The unit does not wake up (reset). I've tried with both the JTAG connected and not connected. Port PA.0 (WKUP pin) has a pull-down resistor, leading to a momentary switch, with Vcc on the other side of the switch, which should be enought to generate the required rising edge when the button is pressed. Any ideas? Thanks!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.