2017-09-10 7:20 AM
In the STM32L4x5/4x6 reference manual (and some other manuals too, like RM0090) the figure 374 shows that the RTC wakeup timer can be clocked with ck_apre, but the description of RTC_CR says that the alternate input is ck_spre.
Can someone confirm that the register description is right and the picture is wrong?
2017-09-11 8:02 AM
Hello
Aaltonen.Juha
,I confirm the typo in the RTC block diagram picture.
RTC_WUTR must receive 2 inputs :
This is a known error reported internallyand will be fixed in coming releases of the reference manual (as for other series of manuals too).
Thanks
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.