2009-01-15 12:47 AM
Retargeting scanf
2011-05-17 3:59 AM
I´m trying to retarget scanf by writing my own fgetc, but I'm having some trouble. The scanf misses the first character in each integer ''sent'' to it. The implementation is the following:
// Just a dummy implementation for debug int fgetc(FILE *f) { static int cnt = 0; int ch; static char str[20] = ''874 543 -345\0\0\0\0''; ch = (int) str[cnt]; cnt = (cnt + 1) % 13; return ch; } main() { int a,b,c; scanf(''%d%d%d'', &a, &b, &c); } When running the code, the result is: a=74, b=73, c=345. If I instead call sscanf(...), the result becomes correct. Any ideas?[ This message was edited by: johan.stridkvist on 15-01-2009 14:37 ]2011-09-23 12:26 AM
Hi Johan,
did you solve this issue? I think I have the same problem with my scanf redirection. The first character or digit sent via a terminal program (hyperterminal or putty) is lost. I am using the IAR Workbench (Kickstart) with a Olimex STM32-P103 Board and the ST-Link v2.2011-09-23 1:46 AM
Hi all,
I use the following scanf retarget and It works fine with IAR : int fgetc(FILE *f) { u16 uiTemp; /* Loop until the end of reception */ while(!(DISPLAY_USARTx->SR & USART_SR_RXNE)); /* Read a character from the USART */ uiTemp = (u16)(DISPLAY_USARTx->DR & (u16)0x01FF); return uiTemp; } void main(void) { u8 uiTemp; printf(''Press 'C' to Continue... :''); scanf(''%c'',&uiTemp); while((uiTemp != 'c') && (uiTemp != 'C')) { scanf(''%c'',&uiTemp); } printf(''\r\n''); }2011-09-23 2:53 AM
Hmm. That is mostly the same way as I implemented it. Are there any configuration changes in the Compiler/Debugger section to edit or any special library includes? Now I've read something about differences between CLib and DLib. DLib uses different routines for printf/scanf (__write and __read). For your information: I am using Workbench version 6.21 with the integrated CMSIS and standard peripheral library version 3.5.0
Here are my versions of fputc and fgetc: int fputc(int iChar, FILE *f) { if(boUSARTen == true) { USART2->DR = (iChar & ((uint16_t)0x01FF)); while((USART2->SR & USART_FLAG_TC) == RESET); /* wait until byte is send */ return iChar; } else { return -1; } } int fgetc(FILE *f) { if(boUSARTen == true) { while(((USART2->SR) & USART_FLAG_RXNE) == RESET);/* wait until data arrived */ return (USART2->DR & (uint16_t)0x01FF); /* return data byte */ } else { return -1; } } Thanks a lot for your help!2011-09-23 6:03 AM
2011-10-11 2:07 AM
Hi Bassem,
I think i have a solution. Iar Workbench 6.21 is using the DLib C-Libraries. In this version you'll have to overwrite the routines __read and __write instead of putchar and getachr! There are two different sets of runtime libraries provided: �? The IAR DLIB Library, which supports ISO/ANSI C and C++. This library also supports floating-point numbers in IEEE 754 format and it can be configured to include different levels of support for locale, file descriptors, multibytes, et cetera. �? The IAR CLIB Library is a light-weight library, which is not fully compliant with ISO/ANSI C. Neither does it fully support floating-point numbers in IEEE 754 format or does it support Embedded C++. (This library is used by default). Migration from CLIB to DLIB There are some considerations to have in mind if you want to migrate from the CLIB library, the legacy C library, to the modern DLIB C/C++ library: �? The CLIB exp10() function defined in iccext.h is not available in DLIB. �? The DLIB library uses the low-level I/O routines __write and __read instead ofputchar and getchar. �? If the heap size in your old compiler version using CLIB was defined in a file named heap.c, you must now set the heap size either in the extended linker command file (*.xcl) or in the Embedded Workbench to use the DLIB library. Source: http://supp.iar.com/FilesPublic/UPDINFO/004350/EWM32C_CompilerReferenceAddendum.pdf
The compiler comes with the IAR DLIB Library, a complete library, compliant with Standard C and C++. This library also supports floating-point numbers in IEEE 754 format and it can be configured to include different levels of support for locale, file descriptors, multibyte characters, et cetera. Source: http://supp.iar.com/FilesPublic/UPDINFO/005832/arm/doc/EWARM_DevelopmentGuide.ENU.pdf Regards Dominik
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.