2020-01-31 12:34 AM
i wrote a program and i want to turn on the led after passing a 500 and 750 , 1000ms.
i use out put compare and use active on mach timer mode.
but it only work one time , i realize that i should reset my timer and count value but i don't know how?
please solve my problem.
thanks in advance.
while (1)
{
HAL_TIM_OC_Start(&htim3,TIM_CHANNEL_1);
HAL_TIM_OC_Start(&htim3,TIM_CHANNEL_2);
HAL_TIM_OC_Start(&htim3,TIM_CHANNEL_4);
HAL_Delay(2000);
HAL_TIM_OC_Stop(&htim3,TIM_CHANNEL_1);
HAL_TIM_OC_Stop(&htim3,TIM_CHANNEL_2);
HAL_TIM_OC_Stop(&htim3,TIM_CHANNEL_4);
sConfigOC.OCMode = TIM_OCMODE_ACTIVE;
sConfigOC.Pulse = 500;
sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
if (HAL_TIM_OC_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
sConfigOC.Pulse = 750;
if (HAL_TIM_OC_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_2) != HAL_OK)
{
Error_Handler();
}
sConfigOC.Pulse = 1000;
if (HAL_TIM_OC_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_4) != HAL_OK)
{
Error_Handler();
}
2020-02-03 4:09 AM
TIMx->CNT = 0;
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.