2020-12-01 9:20 AM
Need 10 samples for a new product prototype. PCBs on the way now. None available in distribution. Can you help?
Thanks - Duncan
2020-12-01 12:03 PM
You might've stated your location, sometimes there are local suppliers which are not tracked globally.
The 'G070 is a lesser-tested cheaper version of the 'G071, of which there appears to be stock worldwide.
JW
2020-12-01 4:41 PM
Jan,
We are located in Northern California. For the product we have designed in the ‘G070CB as it’s a very cost sensitive item. Ideally we would prefer to build and test our prototypes using this part. If the ‘G071CB is a true hardware & firmware drop-in alternative that should be sufficient for our prototype units.
How can we determine if there are ‘G070CB samples available?
Appreciate your help.
2020-12-02 3:36 AM
I am in Central Europe, so for example it's easy for me to get https://uk.rs-online.com/web/p/microcontrollers/1962055/ and even easier https://www.tme.eu/en/details/stm32g070cbt6/st-microcontrollers/stmicroelectronics/ but I don't know whether they are willing to ship to US.
The STM32 models ending with 0 are usually identical chips with the non-0-ending ones, with less testing (which explains the "missing peripherals" - without testing they are as good as nonexistent) and lower temperature range (there may be some other testing -related features missing, e.g. the temperature calibration, or unique ID). The This does not mean ST could not make a dedicated chip with missing features in the future, but generally, you can substitute the "better" chip for the "poorer". The DEV_ID in DBG_IDCODE gives away that it's the same chip.
JW
2020-12-02 3:58 AM
Just to avoid any possible misunderstanding: I am not ST. This is a primarily user-driven forum, with casual ST presence.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.