2018-04-27 3:09 AM
Remap STM32F103 timer input pin.
Help me, please. I'm using stm32103 MCU (LQFP100) and I need PWM input
for measurement of duty cycle.Pin PB0 (TIM3_CH3) is already in use, and I remap TIM3_CH3 to PC8.And I do not get the TIM3_IRQHandler interrupt.GPIOC Pin8: period 20 ms
Could anyone help me find the reason?
Regards,
Anproshfragments of init and interrupt source code -------------------------------------------volatile uint16_t period_capture = 0; volatile uint16_t duty_cycle_capture = 0;volatile uint8_t capture_is_first = 1; volatile uint8_t capture_is_ready = 0;//----------------------------------------------------------- init_timer_temp
void init_timer_temp(void){RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);RCC_APB2PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE);RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOC,ENABLE);GPIO_InitTypeDef GPIO_InitStructure;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;GPIO_Init(GPIOC, &GPIO_InitStructure);GPIO_PinRemapConfig(GPIO_FullRemap_TIM3, ENABLE); //TIM3_CH3 -> GPIOC Pin8
TIM_TimeBaseInitTypeDef timer_base;
TIM_TimeBaseStructInit(&timer_base);timer_base.TIM_Prescaler = 24000 - 1;TIM_TimeBaseInit(TIM3, &timer_base);TIM_ICInitTypeDef timer_ic;
timer_ic.TIM_Channel = TIM_Channel_3;timer_ic.TIM_ICPolarity = TIM_ICPolarity_Rising;timer_ic.TIM_ICSelection = TIM_ICSelection_DirectTI;timer_ic.TIM_ICPrescaler = TIM_ICPSC_DIV1;timer_ic.TIM_ICFilter = 0;// chan1 for period capture chan2 for duty cycle capture
TIM_PWMIConfig(TIM3, &timer_ic);// select trigger source input1 (PC8)TIM_SelectInputTrigger(TIM3, TIM_TS_TI1FP1);TIM_SelectSlaveMode(TIM3, TIM_SlaveMode_Reset);TIM_SelectMasterSlaveMode(TIM3, TIM_MasterSlaveMode_Enable);TIM_ITConfig(TIM3, TIM_IT_CC1, ENABLE);
TIM_Cmd(TIM3, ENABLE);NVIC_EnableIRQ(TIM3_IRQn);}//----------------------------------------------------------- TIM3_IRQHandler
void TIM3_IRQHandler(void){if (TIM_GetITStatus(TIM3, TIM_IT_CC1) != RESET) { TIM_ClearITPendingBit(TIM3, TIM_IT_CC1); NVIC_DisableIRQ(TIM3_IRQn);// capture chan1 chan2
period_capture = TIM_GetCapture1(TIM3); duty_cycle_capture = TIM_GetCapture2(TIM3);NVIC_EnableIRQ(TIM3_IRQn);
if (!capture_is_first)
capture_is_ready = 1;capture_is_first = 0;
if (TIM_GetFlagStatus(TIM3, TIM_FLAG_CC1OF) != RESET)
{ TIM_ClearFlag(TIM3, TIM_FLAG_CC1OF); // ... } }}We’re moving the ST Community to a new platform to give you a better and more reliable community experience.