2024-07-18 12:30 AM
Hi!
Library used: Standard Peripheral Library (Yea, I must use this one)
Hardware:
PORT D PIN 12 Tim4 Channel 1 PORT D PIN 13 Tim4 Channel 2
The test bench frequency/PWM generation is working properly so nothing to debug.
The hardware and cable connections are correct (we already triple-checked them )
The problem arises on the other board: The duty cycle calculated seems to point to only one signal, so if I disconnect the cable of the other signal I still manage to calculate the two duty cycles, meanwhile should go to zero.
Pin 12 Port D Timer 4 Channel 1 configuration:
void myPWM4_Config_1(tmyPWMInput *me)
{
RCC_ClocksTypeDef __RCC_CLOCK;
myPWMInputCtor(me);
RCC_GetClocksFreq(&__RCC_CLOCK);
me->clock = __RCC_CLOCK.PCLK1_Frequency * 2; //APB1
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
me->GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12;
me->GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
me->GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
me->GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
me->GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOD, &me->GPIO_InitStructure);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource12, GPIO_AF_TIM4);
TIM4_IRQHandler_ptf = TIM4_IRQ_PWM;
me->NVIC_InitStructure.NVIC_IRQChannel = TIM4_IRQn;
me->NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;
me->NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
me->NVIC_InitStructure.NVIC_IRQChannelCmd = 1;
NVIC_Init(&me->NVIC_InitStructure);
me->TIM_TimeBaseStructure.TIM_Period = 0xFFFF;
me->TIM_TimeBaseStructure.TIM_Prescaler = 840 - 1;
me->TIM_TimeBaseStructure.TIM_CounterMode=TIM_CounterMode_Up;
me->TIM_TimeBaseStructure.TIM_ClockDivision= TIM_CKD_DIV1;
me->TIM_TimeBaseStructure.TIM_RepetitionCounter = 0;
TIM_TimeBaseInit(TIM4, &me->TIM_TimeBaseStructure);
me->TIM_CH1_ICInitStructure.TIM_Channel = TIM_Channel_1;
me->TIM_CH1_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising;
me->TIM_CH1_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;
me->TIM_CH1_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;
me->TIM_CH1_ICInitStructure.TIM_ICFilter = 0x0;
TIM_PWMIConfig(TIM4, &me->TIM_CH1_ICInitStructure);
// Select the TIM8 Input Trigger: TI1FP1
TIM_SelectInputTrigger(TIM4, TIM_TS_TI1FP1);
// Select the slave Mode: Reset Mode
TIM_SelectSlaveMode(TIM4, TIM_SlaveMode_Reset);
TIM_SelectMasterSlaveMode(TIM4, TIM_MasterSlaveMode_Enable);
// Enables TIM8 peripheral Preload register on ARR.
TIM_ARRPreloadConfig(TIM4, ENABLE);
// Configures the TIM8 Update Request Interrupt source (SETS the CR1->URS bit)
TIM_UpdateRequestConfig(TIM4, TIM_UpdateSource_Regular);
// Enable the CC1 and the update Interrupt Request
TIM_ITConfig(TIM4, TIM_IT_CC1, ENABLE);
TIM_ClearFlag(TIM4, TIM_FLAG_Update);
TIM_Cmd(TIM4, ENABLE);
}
Pin 13 Port D Tim4 Channel 2 configuration:
void myPWM4_Config_2(tmyPWMInput *me)
{
RCC_ClocksTypeDef __RCC_CLOCK;
myPWMInputCtor(me);
RCC_GetClocksFreq(&__RCC_CLOCK);
me->clock = __RCC_CLOCK.PCLK1_Frequency * 2; //APB1
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM4, ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
me->GPIO_InitStructure.GPIO_Pin = GPIO_Pin_13;
me->GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
me->GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz;
me->GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
me->GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOD, &me->GPIO_InitStructure);
GPIO_PinAFConfig(GPIOD, GPIO_PinSource13, GPIO_AF_TIM4);
TIM4_IRQHandler_ptf = TIM4_IRQ_PWM;
me->NVIC_InitStructure.NVIC_IRQChannel = TIM4_IRQn;
me->NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;
me->NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
me->NVIC_InitStructure.NVIC_IRQChannelCmd = 1;
NVIC_Init(&me->NVIC_InitStructure);
me->TIM_TimeBaseStructure.TIM_Period = 0xFFFF;
me->TIM_TimeBaseStructure.TIM_Prescaler = 840 - 1;
me->TIM_TimeBaseStructure.TIM_CounterMode=TIM_CounterMode_Up;
me->TIM_TimeBaseStructure.TIM_ClockDivision= TIM_CKD_DIV1;
me->TIM_TimeBaseStructure.TIM_RepetitionCounter = 0;
TIM_TimeBaseInit(TIM4, &me->TIM_TimeBaseStructure);
me->TIM_CH2_ICInitStructure.TIM_Channel = TIM_Channel_2;
me->TIM_CH2_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising;
me->TIM_CH2_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;
me->TIM_CH2_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;
me->TIM_CH2_ICInitStructure.TIM_ICFilter = 0x0;
TIM_PWMIConfig(TIM4, &me->TIM_CH2_ICInitStructure);
// Select the TIM8 Input Trigger: TI1FP1
TIM_SelectInputTrigger(TIM4, TIM_TS_TI2FP2);
// Select the slave Mode: Reset Mode
TIM_SelectSlaveMode(TIM4, TIM_SlaveMode_Reset);
TIM_SelectMasterSlaveMode(TIM4, TIM_MasterSlaveMode_Enable);
// Enables TIM8 peripheral Preload register on ARR.
TIM_ARRPreloadConfig(TIM4, ENABLE);
// Configures the TIM8 Update Request Interrupt source (SETS the CR1->URS bit)
TIM_UpdateRequestConfig(TIM4, TIM_UpdateSource_Regular);
// Enable the CC1 and the update Interrupt Request
TIM_ITConfig(TIM4, TIM_IT_CC2, ENABLE);
TIM_ClearFlag(TIM4, TIM_FLAG_Update);
TIM_Cmd(TIM4, ENABLE);
}
Capture/Compare Interrupt code:
void TIM4_IRQHandler( void )
{
if (TIM_GetITStatus(TIM4, TIM_IT_CC1) != RESET) {
tmyPWMInput *pPWM4_1 = &myCTRL.myHW.myPortDCfg.myPWM4_1; //PIN12
// Clear TIM8 Capture Compare1 interrupt pending bit
TIM_ClearITPendingBit(TIM4, TIM_IT_CC1);
pPWM4_1->HighPeriod = TIM_GetCapture1(TIM4); // length of high-portion
pPWM4_1->FullPeriod = TIM_GetCapture2(TIM4); // total period
myPWMCalc(pPWM4_1); //Calculate the frequency and duty cycle
}
if (TIM_GetITStatus(TIM4, TIM_IT_CC2) != RESET) {
tmyPWMInput *pPWM4_2 = &myCTRL.myHW.myPortDCfg.myPWM4_2; //PIN13
// Clear TIM8 Capture Compare1 interrupt pending bit
TIM_ClearITPendingBit(TIM4, TIM_IT_CC2);
pPWM4_2->HighPeriod = TIM_GetCapture1(TIM4); // length of high-portion
pPWM4_2->FullPeriod = TIM_GetCapture2(TIM4); // total period
myPWMCalc(pPWM4_2); //Calculate the frequency and duty cycle
}
}
How do I read the two different PWM Signals Duty Cycle I receive from the test bench using only two channels of the same timer? ( the frequency get measured correctly)
Output I get: The two duty cycle i calculate are equal because they point to the same frequency signal, so If I disconnect the cable of the other signal I still read two PWM duty cycles.
What I'm supposed to see: duty cycles similar-ish and when i disconnect one signal the duty cycle of the disconnected signal should go to zero.
2024-07-18 2:47 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.