2020-02-12 7:31 AM
Hello,
can we use the STM32F2 series to read a sound file (e.g. wave file) from a flash or SD card and play ist via I2S?
We would like to transfer the data from the DMA of the SPI into the DMA of the I2S.
Best regards,
Simon
2020-02-14 10:09 AM
Hello,
Please refer to this example that allows playing an audio file with an external codec through the I2S peripheral using DMA transfer :
STM32Cube_FW_F2_V1.8.0\Projects\STM322xG_EVAL\Examples\I2S\I2S_Audio
Best regards
Bouraoui
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.