2012-05-11 6:28 AM
HELLO,
I use
The
STM32L152RBT6
.
I want to know
how I can
read
the logic state
of a pine tree
if it is
up or down
and display it on
LCD.
#!rocketscience2012-05-11 6:53 AM
/* Reads the pin(3) of the GPIOA and store it in ReadValue variable */
u8 ReadValue; ReadValue = GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_3);2012-05-11 6:54 AM
if (
GPIO_ReadInputDataBit(GPIOA
,
GPIO_Pin_3)==0) { [...code...]}
LCD SPI?2012-05-11 7:21 AM
LCD SPI?
Probably not, the STM32L152 can drive the simple glass on it's own. Not sure how the pine tree works, spruce or douglas?2012-05-11 7:26 AM
thank you very much
,
but
is it possible
to give me
the instruction to
display the status
of
pine
on the display
LCD
STM32
board
after
reading it
and
thank you in advance
2012-05-11 7:32 AM
Sorry,
Is this board???STM32L152RBT6 microcontroller featuring 128 KB Flash, 16 KB RAM, 4 KB EEPROM, in an LQFP64 package
On-board ST-Link/V2 with selection mode switch to use the kit as a standalone ST-Link/V2 (with SWD connector for programming and debugging)
Board power supply: through USB bus or from an external 3.3 or 5 V supply voltage
External application power supply: 3 V and 5 V
IDD current measurement
LCD
DIP28 package
24 segments, 4 commons
Four LEDs:
LD1 (red/green) for USB communication
LD2 (red) for 3.3 V power on
Two user LEDs, LD3 (green) and LD4 (blue)
Two pushbuttons (user and reset)
One linear touch sensor or four touchkeys
Extension header for LQFP64 I/Os for quick connection to prototyping board and easy probing
http://www.st.com/internet/evalboard/product/250990.jsp
From: ayari.zied
thank you very much
,
but
is it possible
to give me
the instruction to
display the status
of
pine
on the display
LCD
STM32
board
after
reading it
and
thank you in advance
2012-05-11 7:46 AM
yes it is
the same card
as mine
, so
is
that
you can help me
?
2012-05-11 9:29 AM
I think you need reference the library: stm32l_discovery_lcd
Then use this function to display message at LCD/* Display Welcome message */
LCD_GLASS_ScrollSentence('' **PIN 3 ACTIVE**'',1,SCROLL_SPEED); This funcion can be found at: stm32l_discovery_lcd.c/**
* @brief This function writes a char in the LCD RAM. * @param ptr: Pointer to string to display on the LCD Glass. * @retval None * @par Required preconditions: Char is ASCCI value ''Ored'' with decimal point or Column flag */ void LCD_GLASS_DisplayStrDeci(uint16_t* ptr) { uint8_t i = 0x01; uint8_t char_tmp; // LCD_GLASS_Clear();/* Send the string character by character on lCD */
while ((*ptr != 0) & (i < 8)) { char_tmp = (*ptr) & 0x00ff; switch ((*ptr) & 0xf000) { case DOT:/* Display one character on LCD with decimal point */
LCD_GLASS_WriteChar(&char_tmp, POINT_ON, COLUMN_OFF, i); break; case DOUBLE_DOT:/* Display one character on LCD with decimal point */
LCD_GLASS_WriteChar(&char_tmp, POINT_OFF, COLUMN_ON, i); break; default: LCD_GLASS_WriteChar(&char_tmp, POINT_OFF, COLUMN_OFF, i); break; }/* Point on the next character */
ptr++;/* Increment the character counter */
i++; } } ________________ Attachments : stm32l_discovery_lcd.c : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtDW&d=%2Fa%2F0X0000000aKO%2FFhSOtSxvdFAq6DUKhYrE6hnMtwnlFnyWftoSsjUTpB8&asPdf=falsestm32l_discovery_lcd.h : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtVt&d=%2Fa%2F0X0000000aR6%2FUs8_tSilfLoz7gyKUumW5SKx._7_RWoGFoSo66gJn3Q&asPdf=false2012-05-14 1:53 AM
Again, thank you
,
but I want
the instruction that
allows me to send
the logic state of
pin
PA3 for
example
to
LCD
2012-05-14 10:48 AM
Again, thank you
,
but I want
the instruction that
allows me to send
the logic state of
pin
PA3 for
example
to
LCD
if (GPIO_ReadInputDataBit(GPIOA, GPIO_Pin_3)==0)
LCD_GLASS_DisplayString(''PA3 LOW'');
else
LCD_GLASS_DisplayString(''PA3 HIGH'');
Perhaps you need to review some of the example code for the STM32L Discovery board and get more familiar with programming
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.