2019-08-30 12:58 PM
Hi
I want to read hex file of a STM32F072C8T6 which is installed in a PCB, the board has micro USB port I could connect it and the driver came to device manager it updated with internet automatically, but I need a software to read the hex file then write on new one.
please someone help!!
thanks
2019-08-30 2:16 PM
Well, one possibility is "STM32CubeProgrammer (STM32CubeProg) is an all-in-one multi-OS software tool for programming STM32 products."
2019-08-30 2:38 PM
Yes, if the part has an accessible BOOT pin and ROM firmware supporting USB/DFU mode, you should be able to read/write via STM32 Cube Programmer
2019-08-30 5:35 PM
Thanks
Yes, I got a result but it shows
Warning: Device is under Read Out Protection
what is solution please?
2019-08-30 6:13 PM
>>what is solution please?
Pay the developer for the firmware? The device is copy protected, and presumably not yours.
2019-08-30 7:18 PM
the board is damaged because of damaged MCU I need only change the MCU so I need the program hex file, is there anyway to unlock the protection???
2019-08-31 3:22 AM
No!
2019-08-31 3:24 AM
Ask the device developer for a pre-programmed replacement chip or module.
2019-09-07 5:36 PM
Noted thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.