2022-04-05 5:45 AM
Hello,
I have been working with STM32H7 microcontrollers for a while now but have always used the single core. Now I want to use the Dual core to read and write data in the external SDRAM. I have looked through all materials available online but could not find a particular way.
I have a few other questions
Kindly help me out with these clarifications
Thank you
2022-04-05 6:29 AM
It should access just like any other memory, via its specific address space.
It doesn't "take place simultaneously", one core gets there first, and the accesses are arbitrated by the bus.
For basic inter-core messaging, use the dual-ported RAM, and HSEM as the primary methods.
The SDRAM can be used, but will be relatively less efficient.
Watch cache-coherency, you'd probably want caching on the M7 side, to reduce the latency/penalties, but you could subdivide the MPU space to cached/non-cached.
2022-04-06 5:24 AM
Thank you for your response sir.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.