2025-04-21 2:20 PM - edited 2025-04-21 2:23 PM
I'm generating external interrupts on an WeActStudio STM32F446RET6 board. I've the pins configured as pull-up. When I set one of them to GND, several random interrupts from other pins are generated. For example, if I connect pin PB3 to GND, I get interrupts from PB3 and PB4.
I attach the complete project, I'm compiling it with Visual Studio Code.
What could be the cause?
My callback function is:
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {
static uint32_t last_interrupt_time[6] = {0}; // For multiples pins
uint32_t current_time = HAL_GetTick();
#define debounce_time 50 //ms
switch(GPIO_Pin) {
case GPIO_PIN_0:
if (current_time - last_interrupt_time[0] > debounce_time) {
last_interrupt_time[0] = current_time;
printf("INT PB0\r\n");
}
break;
case GPIO_PIN_1:
if (current_time - last_interrupt_time[1] > debounce_time) {
last_interrupt_time[1] = current_time;
printf("INT PB1\r\n");
}
break;
case GPIO_PIN_3:
if (current_time - last_interrupt_time[2] > debounce_time) {
last_interrupt_time[2] = current_time;
printf("INT PB3\r\n");
}
break;
case GPIO_PIN_4:
if (current_time - last_interrupt_time[3] > debounce_time) {
last_interrupt_time[3] = current_time;
printf("INT PB4\r\n");
}
break;
case GPIO_PIN_5:
if (current_time - last_interrupt_time[4] > debounce_time) {
last_interrupt_time[4] = current_time;
printf("INT PB5\r\n");
}
break;
case GPIO_PIN_6:
if (current_time - last_interrupt_time[5] > debounce_time) {
last_interrupt_time[5] = current_time;
printf("INT PC6\r\n");
}
break;
default: break;
}
}
Solved! Go to Solution.
2025-04-21 2:24 PM
Several EXTI dump into the same Handler?
HAL dispatchs in a shot-gun method rather than qualifying?
You've got noise or signal bounce on your inputs?
TIM pins in input capture might provide additional filter and clock options.
2025-04-21 2:24 PM
Several EXTI dump into the same Handler?
HAL dispatchs in a shot-gun method rather than qualifying?
You've got noise or signal bounce on your inputs?
TIM pins in input capture might provide additional filter and clock options.
2025-04-21 11:08 PM
Shared EXTI Handlers: Yes, I’m aware that EXTI9_5 shares one handler (for pins 5-9), but my issue also occurs with PB3 (EXTI3) and PB4 (EXTI4), which have dedicated handlers (EXTI3_IRQHandler/EXTI4_IRQHandler).
Noise/Bouncing: I already had software debounce implemented (50ms delay in callbacks), I've now added hardware debouncing (1kΩ series resistor + 100nF capacitor to GND) on a pin. It works! I didn't know that noise on a single pin can trigger interrupts on other pins.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.