2009-06-02 1:42 AM
Questions about STM32 project
2011-05-17 4:13 AM
Hello to all,
I'm new to SMT32 and I'm going to make a large project which involves a PC and two separate boards with two STM32F103RE on-board. The PC will be connected to the first board through USB. The two boards will be connected through a serial communication (RS232 or RS485). I'm wondering if I can handle the following features: * firmware upgrade: via USB for the first board, via USB + serial to reach the second one. The download should begin after a software command, I can't use a push button to start the upgrade routine. * I need two separate serial channels on the USB connection (between the PC and the first board) at 115200, 8N1. Do you think these key points are easily handled? ;) Thanks! Marco Trapanese Italy [ This message was edited by: info89 on 02-06-2009 13:26 ]2011-05-17 4:13 AM
Quote:
I'm new to SMT32 and I'm going to make a large project...
It is usually more sensible to start with a small project, and work up from there. Whatever you do, don't try to build the whole thing, then switch it all on and hope that it works. Do it step-by-step; eg, Start with a ''simple'' (sic) USB connection from one STM32 to a PC; Build yourself some diagnostic features over that link - printf, etc. and so on, step-by-step...Quote:
I'm wondering if I can handle the following features:
* firmware upgrade: via USB for the first board, via USB + serial to reach the second one. The download should begin after a software commandNo problems. You should treat the software update and the data transfer as separate functions - the updater shouldn't care how the data arrrives.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.