2009-03-06 8:31 AM
Question about the generated hex file
2011-05-17 4:05 AM
I'm sitting here analyzing the Ride7 generated hex file (intel hex32 format) because I'm going to make a bootloader.
What does this row do? :04000005080021309E It breaks up to these: : Start code 04 Byte count: 4 0000 Address 05 Record type: Start Linear Address Record 08002130 <--- is this a start address? 9E Checksum Does it say the execution start address is 0x08002130? Just curious. I don't think I need to decode this record type for extracting the FLASH memory map.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.