2014-03-31 1:45 AM
I am using the TIM1 in the stm32f4 in encoder interface mode to get position. The two chanels of my rotary quadrature encoder are connected to the pins A8 and A9 through a comparator. The outputs from the comparator can be seen as two nice square waves on a scope.
At low speeds the timer counts perfectly well. But at slightly moderate speeds the timer losses a lot of counts and does not work properly. At high speeds it performs very badly. I configured the GPIO pins as such;GPIO_InitTypeDef GPIO_InitStructure;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8 | GPIO_Pin_9;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource8, GPIO_AF_TIM1);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_TIM1);
The timer was configured as such;
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_TimeBaseStructure.TIM_Prescaler = 0;
TIM_TimeBaseStructure.TIM_Period = 0xFFFFFFFF; // Maximal
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM1, &TIM_TimeBaseStructure);
TIM_EncoderInterfaceConfig(TIM1, TIM_EncoderMode_TI1, TIM_ICPolarity_Rising, TIM_ICPolarity_Rising);
TIM_Cmd(TIM1, ENABLE);
Why is the timer loosing counts?
Should I also configure input capture for the two channels of TIM1?
What am I doing wrong here?
#stm32f4 #discovery #encoder-interface #timers #qei
2014-04-22 10:36 AM
Mine wouldn't work properly even at fairly low speeds, with
GPIO_Speed_2MHz.
I changed to 10MHz and it improved quite a bit.
Bill
2014-04-22 12:24 PM
Check your digital filter setting:
TIM_ICInitStructure.
TIM_ICFilter
in the timer configuration. I use rotary optical encoders, single ended on a short cable, at up to 40KHz with a filter setting of 5 and GPIO at 2MHz. I see attenuation when running at higher filter settings so you may need to check the filter calculations for whatever speed your inputs run at. Jack Peacock2014-04-23 5:46 AM
You might also want to check the hardware side of your setup. If the wires are too long or there is unexpected capacitance or inductance in the circuit the square wave output from the encoder could be turned into spikes too short for the MCU to identify.
Just a thought.2014-04-23 6:01 AM
Any chance you could paste in some code on how you configure this filter?
I'm not using TIM_ICInitTypeDef at all currently. BillWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.