2008-11-18 2:27 AM
Pull-up/down on Output pins?
2011-05-17 3:52 AM
Is it possible to configure an output WITH internal pull-up or pull-down? It would save some parts in SDIO and I2C....
From what I see in stm32f10x_gpio.h, the PU and PD are only availlable on inputs... Is it correct, or is there a way? #define IS_GPIO_MODE(MODE) (((MODE) == GPIO_Mode_AIN) || ((MODE) == GPIO_Mode_IN_FLOATING) || ((MODE) == GPIO_Mode_IPD) || ((MODE) == GPIO_Mode_IPU) || ((MODE) == GPIO_Mode_Out_OD) || ((MODE) == GPIO_Mode_Out_PP) || ((MODE) == GPIO_Mode_AF_OD) || ((MODE) == GPIO_Mode_AF_PP)) -Jay2 [ This message was edited by: relaxe on 18-11-2008 15:58 ]We’re moving the ST Community to a new platform to give you a better and more reliable community experience.