2015-11-15 2:34 PM
I have a Nucleo F411RE board and eventually want to program it with code generated by the MikroE Pascal for ARM compiler. At present I have the board running code from the MBed C++ compiler and the programming side of this is great. To program the device by copying the binary file to a ''disk'' that is in fact the development board programmer is very convenient.
Eventually however, I want to get code from the MikroE compiler into the board. MikroE have a programmer (which we have bought), however the programmer has a JTAG interface and I can't see how we would interface this to the Nucleo. I don't necessarily want to go that way however - if I can utilize the convenience of the ''copy-a-binary-file-to-program-the-device'' and avoid the need to hook up a programmer (when the Nucleo already has one on board) it would be sweet.And so to my question(s):2015-11-15 5:13 PM
I suspect you can answer a lot of your own questions if you do a little experimentation, and review the outputs with a file manager, hex editor, or whatever tools of choice you use.
You can use the ST-LINK Utilities to read off the content of the F411RE, and verify for yourself what's on it. Similarly it can be used to write data to the board independent of mbed. I don't have MikroE compilers, but have a number of their boards, including the Clicker 2, click boards, and F4-DISCO breakout boards, and the ST-LINK V2 mikroProg adapter.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.