2022-03-21 11:15 PM
Bir projemde stm32l052 kullanmaktayım ve işlemci pin sayım yetersiz gelmekte. Acaba programlama pinlerini programlama yapmıyorken gpio olarak kullanabilirmiyim?
2022-03-22 2:56 AM
Hello @Snm.1 and welcome to the Community :)
Please try to write in English if you want to get an answer, because most of the people on this community can speak English but not Turc.
I used Google translate to get an rough idea of what you are saying :
"Extra features of programming pins.
I am using stm32l052 in a project and my processor pin count is insufficient. I wonder if I can use the programming pins as gpio when not programming?
"
You have the possibility to use the GPIO and select alternate functions inputs/outputs. You should check the GPIO pins in the datasheet of your product.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Thanks
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.