2012-03-29 2:33 AM
Hello to all,
I have stm32-h107 board, i use eclipse and yagarto toolchain (my OS is windows7). I want to use the feature usb on the go to establish communication with my laptop. i downloaded the driver for virtual com port and installed it in my laptop. Afterwards, i compiled the example ''Virtual_COM_Port'' ( taken from ''STM32_USB-FS-Device_Lib_V3.3.0''), and compiling gave no errors. The problem rises as i start the debugging : code 43 pops up, that is ''Windows has stopped this device because it has reported problems''. I check Device Manager and there is an ''Unknown Device'' under Universal Serial Bus Controllers with an exclamation mark. I load to this device the inf file that i have already installed, but nothing changes.Any ideas are welcome!Best regards,Dion2012-03-29 5:21 AM
You should write *.inf script file.Without this plug and play process does not work right
2012-03-29 5:56 AM
thank you very much for the reply! i am newbie so i lack of experience. i will implement your idea.
Best regards,DionWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.