2015-10-16 12:36 AM
i am workin on diplaying no''s on 7 segment via stm32f072b
the problem is that the o/p is not appearing on the 7 segment ive connected pins of 7 seg to gpioA and gpioC via a 3.3k resistor the follwing is the code#include ''main.h''
//------------------------------------------------------------------------------ // Function Name : Init _GPIO pins // Description : pins ,port clock & mode initialization. //------------------------------------------------------------------------------ void Init_GPIO(void) { /* GPIO config */ GPIO_InitTypeDef GPIO_InitStructure; /* GPIOA GPIOB clock enable */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOA | RCC_AHBPeriph_GPIOC, ENABLE);/* Configure 8 ,9 PINS as input floating */
GPIO_InitStructure.GPIO_Pin =GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 ; /* Configure PORT clock speed */ GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz; /* Configure PORT mode as input */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; /*configure PINS to output pushpull mode*/ GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; /* Above all GPIO instructions apply to port ''C''*/ GPIO_Init(GPIOC, &GPIO_InitStructure);/* Configure 8,9,10,11,12,13 pins as input floating */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3 ; ; /* Configure PORT clock speed */ GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz; /* Configure PORT mode as input */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; /*configure PINS to output pushpull mode*/ GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; /* Above all GPIO instructions apply to port ''B''*/ GPIO_Init(GPIOA, &GPIO_InitStructure); }/*******************************************************************************
* Function Name : main * Description : Main program. *******************************************************************************/ int main(void) { Init_GPIO(); //calling a function while(1)//infinite loop { /*ODR bits can be individually set and reset */ //for displaying 0 GPIOA->ODR = 0x0007; GPIOC->ODR = 0x0007; } }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.