2014-07-07 1:19 PM
Hi,
I am using STM3220G-SK to read adc values from an external source.I have tried different codes but all of them give me the same result. once the program is fired the adc valued is read and shown on the LCD but after that the value will remain unchanged regardless of the voltage change. to read the new value I have to either enter debugging mode again or turn off/on the module.could anyone let me know where I am making a mistake. I have not so much experience in embedding programming and I have just started to work in this area.Thanksmy code is written below:int main(void){GPIO_InitTypeDef GPIO_InitStructure;ADC_InitTypeDef ADC_InitStructure;DMA_InitTypeDef DMA_InitStructure; ADC_CommonInitTypeDef ADC_CommonInitStructure;__IO uint16_t Adcdata [2] ; RCC_AHB1PeriphClockCmd(TRIMER_CLK, ENABLE); GPIO_InitStructure.GPIO_Pin = TRIMER_PIN; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(TRIMER_PORT, &GPIO_InitStructure); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2| RCC_AHB1Periph_GPIOC | RCC_AHB1Periph_GPIOA , ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC2, ENABLE); DMA_StructInit(&DMA_InitStructure); DMA_DeInit(DMA2_Stream4); DMA_InitStructure.DMA_Channel = DMA_Channel_0; DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)ADC1_DR_ADDRESS; //Source address*/ DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&Adcdata[1]; //Destination address*/ DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory; DMA_InitStructure.DMA_BufferSize = 2; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; DMA_InitStructure.DMA_Mode = DMA_Mode_Circular; DMA_InitStructure.DMA_Priority = DMA_Priority_High; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; DMA_Init(DMA2_Stream4, &DMA_InitStructure); //Initialize the DMA DMA_Cmd(DMA2_Stream4, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOC, &GPIO_InitStructure); ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ScanConvMode = ENABLE; ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent; ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles; ADC_CommonInit(&ADC_CommonInitStructure); ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_NbrOfConversion = 1; ADC_Init(ADC2, &ADC_InitStructure); ADC_Init(ADC1, &ADC_InitStructure);ADC_RegularChannelConfig(ADC2, ADC_Channel_15, 1, ADC_SampleTime_144Cycles); ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE); ADC_DMACmd(ADC2, ENABLE); ADC_Cmd(ADC2, ENABLE); ADC_SoftwareStartConv(ADC2);ADC_ITConfig(ADC2, ADC_IT_EOC, ENABLE);while(1) { if (ADC_GetFlagStatus(ADC2, ADC_FLAG_EOC) == RESET); { Adcdata[0] = ADC_GetConversionValue(ADC2); ADC_DMARequestAfterLastTransferCmd(ADC2, ENABLE); GLCD_print(''%d'', Adcdata[0]); ADC_ClearFlag(ADC2, ADC_FLAG_EOC); DelayResolution100us(10000); /* Start ADC1 Software Conversion */ ADC_SoftwareStartConv(ADC2); }}while(1){}; #adc #dma2014-07-07 2:36 PM
Yes, all rather a mess there.
Using DMA, or polling? Using ADC1 or ADC2? One channel or two? Independent or Simultaneously? Initial element of array adcdata[0] not adcdata[1][DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/3%20channels%20on%20ADC1%20and%20DMA&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=690]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2F3%20channels%20on%20ADC1%20and%20DMA&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=690[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/stm32f207%20ADC%2BTIMER%2BDMA%20%20Poor%20Peripheral%20Library%20Examples&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=2642]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2Fstm32f207%20ADC%2BTIMER%2BDMA%20%20Poor%20Peripheral%20Library%20Examples&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=2642 See also STM32F2xx_StdPeriph_Lib_V1.1.0\Project\STM32F2xx_StdPeriph_Examples\ADC2014-07-09 4:15 PM
Thank you very much for your reply,
I was trying to use two different ADCs at the same time, I have cleaned the code and I am using only one channel of ADC2 to read an external value. My neat code is below, however, the ADC does not change by changing voltage and it is constantly 1 v regardless of true value.int main(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
ADC_InitTypeDef ADC_InitStructure;
DMA_InitTypeDef DMA_InitStructure;
ADC_CommonInitTypeDef ADC_CommonInitStructure;
__IO uint16_t Adcdata=0 ;
RCC_AHB1PeriphClockCmd(TRIMER_CLK, ENABLE);
GPIO_InitStructure.GPIO_Pin = TRIMER_PIN;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(TRIMER_PORT, &GPIO_InitStructure);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2| RCC_AHB1Periph_GPIOC, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC2, ENABLE);
DMA_StructInit(&DMA_InitStructure);
DMA_DeInit(DMA2_Stream3);
DMA_InitStructure.DMA_Channel = DMA_Channel_1;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)ADC2->DR; //Source address*/
DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&Adcdata; //Destination address*/
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;
DMA_InitStructure.DMA_BufferSize = 1; //Buffer size
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; //source size - 16bit
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; // destination size = 16b
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA2_Stream3, &DMA_InitStructure); //Initialize the DMA
DMA_Cmd(DMA2_Stream3, ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AIN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOC, &GPIO_InitStructure);
/*ADC2 configuration*/
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ScanConvMode = DISABLE;
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;
ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;
ADC_CommonInit(&ADC_CommonInitStructure);
ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;
ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_NbrOfConversion = 1;
ADC_Init(ADC2, &ADC_InitStructure);
/*ADC2 regular TRIMER_CHANNEL configuration*/
ADC_RegularChannelConfig(ADC2, ADC_Channel_15, 1, ADC_SampleTime_56Cycles);
ADC_Cmd(ADC2, ENABLE);
ADC_DMARequestAfterLastTransferCmd(ADC2, ENABLE);
ADC_DMACmd(ADC2, ENABLE)
ADC_SoftwareStartConv(ADC2);
ADC_Cmd(ADC2, ENABLE);
ADC_DMARequestAfterLastTransferCmd(ADC2, ENABLE);
ADC_DMACmd(ADC2, ENABLE);
ADC_SoftwareStartConv(ADC2);
GLCD_Backlight(BACKLIGHT_ON);
while(1)
{
GLCD_print(''%d'', Adcdata);
}
while(1){}
}
Thanks2014-07-09 5:45 PM
I don't have a manual/schematic for your board, will assume the POT/TRIMMER is on PC5
Are you should there aren't any jumpers on the board precluding the ADC from reading the voltage? Probably wouldn't put DMA data on the stack2014-07-10 2:00 PM
2014-07-17 9:08 AM
2014-07-17 10:28 AM
Actually the main problem is reading 0 , it does not give a stable zero reading but the the highest voltage is exactly 3.3 volts
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.