2019-09-04 12:38 AM
I am try to connecting a STM32 Nucleo (F401RE) to a ESP8266 on UART.
I've managed to control the ESP8266 with the PC using a usb/uart channel and hyperterminal.
I've managed to send uart messages to the PC from the Nucleo
But I am unable to command the ESP8266 from the Nucleo, the same commands that worked sent from my PC, do not work sent from the Nucleo.
I've sent a simple char 't' just to see how it looks on the scope from both PC and Nucleo to comapre, and Im attaching my measurements, There is a difference between the usb/uart device and what the Nucleo sends, an Endian, it seems the Nucelo adds some '0' and I suspect this might cause the problem.
this is my configuration of the Nucleo channel
huart1.Instance = USART1;
huart1.Init.BaudRate = 115200;
huart1.Init.WordLength = UART_WORDLENGTH_8B;
huart1.Init.StopBits = UART_STOPBITS_1;
huart1.Init.Parity = UART_PARITY_NONE;
huart1.Init.Mode = UART_MODE_TX_RX;
huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart1.Init.OverSampling = UART_OVERSAMPLING_16;
I would appreciate some insights on this issue
Thanks!
Solved! Go to Solution.
2019-09-04 6:49 AM
Show your code that actually sends the data from the Nucleo. I bet it looks something like this:
char cmd[] = "t"; // This is actually 2 bytes, 't' and '\0'
HAL_UART_Transmit( huart1, cmd, sizeof(cmd) ); // therefore, sizeof() is 2
2019-09-04 6:49 AM
Show your code that actually sends the data from the Nucleo. I bet it looks something like this:
char cmd[] = "t"; // This is actually 2 bytes, 't' and '\0'
HAL_UART_Transmit( huart1, cmd, sizeof(cmd) ); // therefore, sizeof() is 2
2019-09-04 9:23 AM
You sir are a national treasure of whatever nation you belong to.
Now it is working.
Have a great day.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.