2018-01-03 1:16 AM
Hello, I am new to STM 32 devices so go easy. I would like to port over the IAP included in the AN4854 which is for a STM32072B Evaluation board over to a STM32f746 Discovery board. I have read through the application note a few times. I have previous experience with IAP on other devices so the memory mapping is not the issue....at the moment. What I am struggling on is after changing the device name, my understanding is I then have to change the HAL drivers. What is the best way to go about this without incurring lots of errors?
Thank you
#stm32-f7 #stm32f7-hal #stm32-iap2018-01-04 12:59 AM
STM32072B Evaluation board
So an STM32F072VBT6 microcontroller, then?
http://www.st.com/en/evaluation-tools/stm32072b-eval.html
So Cortex-M0
to a STM32f746
Which is Cortex-M7.
Is there not something closer to start with?
after changing the device name
Where?
You haven't said what tools you are using.
change the HAL drivers
Yes - you will need the particular HAL drivers for the chip in question.
The easiest way is often (usually?) to start a fresh project
for the chip in question, and merge/port other code into that ...
2018-01-04 2:24 AM
Thanks for the reply.
I am totally new to ST chips so please forgive me. I was advised to use the IAP example then port it over to the correct device.
I am using system workbench for STM32. I have also created another project using STM32CubeMX.
I have used an example project for the
STM32f746 Discovery board and create my own application which include a display.
So would it be better to create my own project using
STM32CubeMX, then add in the function and header files which are needed for the IAP. I can then set the correct locations in the linker for my application.
2018-01-04 3:42 AM
Some suggestions here:
https://community.st.com/0D50X00009XkXMoSAN
2018-01-04 4:26 AM
Daniel Hatcher wrote:
I am totally new to ST chips so please forgive me.
Not really specific to ST.
While the Flash subsystem (and other peripherals) is not directly related to the core type, my point with Cortex-M0 vs M7 is that M0 is 'bottom of the range', and M7 'top of the range' - so it is quite likely that an M7-based chip will probably also have a 'beefed-up' flash subsystem to match.
I was advised to use the (sic?) IAP example
Who advised?
I think there are several IAP examples - have you checked if there's one specifically for the
STM32f7...
?
would it be better to create my own project using
STM32CubeMX, then add in the function and header files which are needed for the IAP.
Probably.
then set the correct locations in the linker for my application.
That's probably not the only thing that'll need changing ...
2018-01-04 5:17 AM
Slightly different FLASH banking options, but a bit closer on target..
Repository\STM32Cube_FW_F7_V1.8.0\Projects\STM32F769I_EVAL\Applications\IAP
If you've written bootloaders before you might want to see if that is a better starting point, and merge in the FLASH/ST specific stuff. Review how the FLASH is organized via the Reference Manual. Most concepts from other ARM architectures are highly portable to ST's implementations. From a PIC, AVR or 8051 the scale and organization perhaps more dramatically different.
2018-01-05 12:16 AM
Thank you very much for the help. I will crack on today with your suggestion to start with the project located...
Repository\STM32Cube_FW_F7_V1.8.0\Projects\STM32F769I_EVAL\Applications\IAP and give you an update later on. Thanks
2018-01-08 7:29 AM
I have created a project for my board. I can erase and write to a single address then read the address to check that the value has been written correctly which is does. I have then used the function in the examples for writing the whole file to flash and incrementing the address. I have also used a jump to application function for after the flashing. However, after flashing and jump to application the code does not seem to run.
I know that my jump to application function is correct, because if I set the address to jump to the start i.e.0x08000000. The code will then start to reflash and continue in this loop of erase/flash/jump to start.
So it seems to be something to do with my writing. Below is my writing to flash function.
__IO uint32_t read_size = 0x00, tmp_read_size = 0x00;
uint32_t read_flag = TRUE;/* Erase address init */
LastPGAddress = APPLICATION_ADDRESS;/* While file still contain data */
while (read_flag == TRUE) {/* Read maximum 'BUFFERSIZE' Kbyte from the selected file */
if (f_read(&MyFile, RAMBuf, BUFFERSIZE, (uint_t*) &read_size) != FR_OK) {}
/* Temp variable */
tmp_read_size = read_size;/* The read data < 'BUFFERSIZE' Kbyte */
if (tmp_read_size < BUFFERSIZE) { read_flag = FALSE; }/* Program flash memory */
if (FLASH_If_Write(LastPGAddress, (uint32_t*) RAMBuf, read_size) != FLASHIF_OK) {}
/* Update last programmed address value */
LastPGAddress = LastPGAddress + tmp_read_size; }f_close(&MyFile);
I have set my linker scripts to the following
Bootloader
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 64K
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 320KApplication
FLASH (rx) : ORIGIN = 0x08010000, LENGTH = 960K
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 320K#define VECT_TAB_OFFSET 0x10000
I am jumping to the address
0x08010000 too.
Is there a way back to read the device once programmed to see what exactly has been programmed and where? Any help on why my writing function does not work too would be greatly appreciated.
________________ Attachments : mainV2.c.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyD0&d=%2Fa%2F0X0000000b4c%2FBkHcWeL_ATbzxhmN9E3TT6SW2B2Ydxvxx9bbgKbIsoE&asPdf=false2018-01-08 8:43 AM
The ST-LINK Utilites can read back the device content. You could also save content back onto the SDCard.
Would tend to CRC the data written to FLASH and compare that to the binary file I generated in the linker. Use serial port to output progress/telemetry.
The debugger should permit you to walk into your own code. Have a Hard Fault handler that outputs diagnostics if you end up there, and make sure SCB->VTOR is actually set properly. ie use SCB->VTOR = &__Vectors; rather than the VECT_TAB_OFFSET nonsense.
2018-01-08 9:17 AM
I have used the ST LINK Utilites software and have found that as I suspected the application is not being flashed. I have debugged the function and it fails due to
if (tmp_read_size < BUFFERSIZE) {
read_flag = FALSE;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.