2017-09-21 2:17 AM
Hello,
I need bluetooth module in my project. I start my project using cubeMX for stm32L476ZE and after that project exported to keil. Other basic operations are working fine(Led bliking, button press). I have successfully added some modules like reading data from external sensors using SPI and ADC etc simply looking at some examples avialable from the internet. Now I need a bluetooth module which will be communicate via SPI3 channel. I am trying to porting it from the example SensorDemo. I added the Middlewares for STM32_BlueNRG. But its not working and I have someissues.
I am getting a warning in ble_list.c :
uwPRIMASK_Bit = __get_PRIMASK(); /**< backup PRIMASK bit */
__set_PRIMASK(uwPRIMASK_Bit); /**< Restore PRIMASK bit*/
'
warning: Implicit declaration of function is invalid in c999
' -- while the same is working on the given example project.My question is what is the simplest way to proting a bluetooth module in my project ?
#st-bluetoothWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.