2015-05-25 4:13 AM
Hello
What is range of the PLLN and PLLI2SN multiplication factors?According to pages 226 and 265 of RM0090_Rev9, their range is 192=< PLLN , PLLI2SN <= 432 , so factors below 192 aren't allowed?Thanks.2015-05-25 6:40 AM
The VCO has a range of 192-432 MHz, and a comparison frequency for the PLL in the 1-2 MHz range.
The value N here assumes a 1 MHz comparison. What's happening here is division, technically not multiplication.2015-05-25 7:38 AM
So what to do with this recommendation that the comparison frequency must be 2MHz to limit jitter?
2015-05-25 11:32 AM
So are you measuring a lot of jitter now?
You'd set the PLL/VCO up so it's internal frequency falls in the 192-432 MHz range. So a multiplier of 96-216 from the 2 MHz comparison frequency.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.