2011-02-27 5:25 PM
PLL isn't lock at using HSI
2011-05-17 5:26 AM
Check your initial conditions. Dump them out, and along the way so people can at least figure out what might be amiss.
Check that HSI is running, and ready, and the source clock. Make sure you mask the CFGR properly when setting HCLK, PCLK1/2 Try using the library code.2011-05-17 5:26 AM
Hello clive1
The PLL ready after power down all systems.
It was a rudimentary mistake...
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.