cancel
Showing results for 
Search instead for 
Did you mean: 

PA9(USART1_TX) & PA10(USART1_RX) pin failure in STM32F107RBT

amitpatil
Associate
Posted on January 13, 2015 at 11:02

-I have observed PA9(USART1_TX) & PA10(USART1_RX) pin failure in STM32F107RBT, this pins are 5V Tolerant-FT

- STM32 supply voltage is 3.3V

- it is interfaced to another micro controller which runs on 5V.  
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on January 13, 2015 at 14:21

Damaged/failed permanently?

Proper common ground?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.