2019-07-12 6:56 AM
I'm trying to use both internal op-amps to sample analog inputs with ADC1 and ADC2. When the op-amps are setup using CubeMX (latest version), 3.3v stays present on PA6 input. PA0 works as expected. Both ADCs sample correctly but the waveform input through OPAMP2 is biased up.
I lifted pin 42 (PA6) and the pin reads 3.3 vdc with NOTHING CONNECTED to it. It's clearly a setup problem!
What is the procedure to enable both OPAMPS using CubeMX?
I've tried everything on 2 different boards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.