2022-03-23 11:22 AM
I would like to know if the following is possible and if so, where can I find information about it.
I have a STM32L010K8 micro connected via USART to an LTE CHIP (BG96) through which I can get the firmware update that runs on the microcontroller. I could overwrite the firmware of the micro STM32 to update it automatically.
2022-03-23 11:26 AM
Mostly limited by your own creativity and capabilities.
Should be able to pull data via modem using HTTP, FTP or other protocols.
You'd probably want to have a small, minimal, loader capable to connecting and updating, outside of the larger application.
Do you have any local memory with which to stage complete updates?
2022-03-24 8:47 AM
Thanks for the reply.
The BG96 has physical memory where I can store the firmware update for the microcontroller that I receive via HTTP.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.