2018-07-06 7:24 AM
Has anyone ever tried to program STM32F469 discovery board using OpenOCD?
I am receiving the following error. Any ideas to debug this or any leads on this is appreciated.
embedded:startup.tcl:21: Error: Command/target: stm32f4x.cpu Exists
in procedure 'script' at file 'embedded:startup.tcl', line 60in procedure 'target' called at file './tools/OpenOCD/stm32f4x.cfg', line 71in procedure 'ocd_bouncer' at file 'embedded:startup.tcl', line 21#openocd #stm32f469-discovery2018-07-06 7:45 AM
Yeah, so look at the lines it is complaining about, or provide them as context to the question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.