2008-08-06 8:49 PM
only one breakpoint can be set?
2011-05-17 3:41 AM
This question should be related to IAR EWARM,
but I do not know the place of the IAR forum, the question is while enter debugging, the message below shown, or refer to attached file. The C-SPY option ''Run to 'main''' is enabled,but due to a lack of breakpoints this will require single-stepping ,which may take a long time. Do you want to execute anyway,or stop at the first instruction? only one breakpoint can be set under this condition! why and how to get it right?2011-05-17 3:41 AM
which device are using(STM32, STR9,..)? BTW with the STM32 you can set more than 2 breakpoints.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.