2022-12-23 5:00 AM
Hello,
While trying to setup an UART connection with a STM32U585ZIT6, we realized that it was not possible to drive the G connectors. To isolate the issue we tried to drive others GPIOs and they are totally fine while GPIOs G remain stuck at GND.
We created a new project from STM32Cube and only activated some GPIO to ensure that they are all working except the GPIOs G.
We added the following lines to the output of STMCube :
while (1)
{
HAL_Delay(1000);
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_6, GPIO_PIN_SET); //does not drive
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_SET); // drive
HAL_Delay(1000);
HAL_GPIO_WritePin(GPIOG, GPIO_PIN_6, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_SET);
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}Best regards,
Corentin
2022-12-23 5:10 AM
Sounds like you need to enable VDDIO2
2022-12-23 5:14 AM
Hello,
Thank you for the quick reply. I forgot to precise that we checked that VddIO2 is well enabled through SystemPower_Config that is called in the main (as in the output of STM32Cube).
static void SystemPower_Config(void)
{
HAL_PWREx_EnableVddIO2();
}I just observe that I also forgot to precise that a colleague is able to drive the GPIOG on the same hardware by using an anterior version of STM32IDE.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.