2019-05-28 12:39 AM
I want use external memory IC(IDT 7204 FIFO memory)
I use two STM32H743II(one is write FIFO, one is read FIFO)
I think read was good work.
but write is not good.
I set FMC LCD Interface like Cubeset picture
I think one data write operation, NWE pulse appear 1 time.
but when one data write, 4 NWE pulse shown.(refer tek0009 scope data)
write code is like below.
*(__IO uint16_t *) FIFO_D = rCnt;
4 NWE pulse is normal status?
2019-05-28 12:59 AM
All signals for static memories and similar parallel interfaces are qualified by the NEx (chipselect) signal, so you should observe also that signal.
JW
2019-05-28 1:21 AM
NE1 is two pulse.
why 2 pulse?
2019-05-28 1:35 AM
Well, I don't know.
Does the address/data remain the same, i.e. does it write the same data to the same address twice? If yes, it can't be considered an error - static memories wouldn't care about it, it's just ineffective. It even may be documented - look into the errata.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.