2008-06-05 12:25 AM
NVIC FAST DISABLE ENABLE
2011-05-17 3:36 AM
Hi,
What is the way most fast to enable or disable an interrupt exti? The interrupt that i use is EXTI_Line1, EXTI_Line11. The compiler that i use is Ride7. In the library of NVIC i find this: for enable NVIC->ISER[(NVIC_InitStruct->NVIC_IRQChannel >> 0x05)] = (u32)0x01 << (NVIC_InitStruct->NVIC_IRQChannel & (u8)0x1F); for disable NVIC->ICER[(NVIC_InitStruct->NVIC_IRQChannel >> 0x05)] = (u32)0x01 << (NVIC_InitStruct->NVIC_IRQChannel & (u8)0x1F); so i change it with this value for example (exti1): NVIC->ISER[(0X07 >> 0x05)] = (u32)0x01 << (0X07 & (u8)0x1F); but it is this error error: 'NVIC_TypeDef' has no member named 'ISER' What can I do? Thanks.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.