2021-05-25 6:43 AM
hello all,
I try to use the arm lib to make a FFt but I d'ont understand it well and so I can't.
I need some help on it.
first, I make a acquisition of a signal (form a generator).
the signal is at 30KHz.
I sample with the STM32 at 1MHz.
I use a DMA to add and transert the signal to the DAC
now I want to know precisely the frequency of the signal, so I think to use FFT.
I init the fft cmd,
arm_rfft_fast_init_f32(&fft_handler, 4096);
and then, use this one
arm_rfft_fast_f32(&fft_handler, adc_val, fft_out_buf,0);
I don't understand after that how to found the frequency of my signal.
edit, sorry the message was created empty
2021-05-25 6:45 AM
Is there a question?
The CMSIS directories for CubeL4 will contain the DSP library, this is usable on CM4 parts.
2021-05-25 6:52 AM
yes sorry I click to quickly. I edit it now
2021-05-25 7:59 AM
This seems like a general DSP question about how one uses an FFT rather than something specific about how the ARM Math library's FFT implementation works. That's a bit off-topic for this forum. A better place for this question may be dsp.stackexchange.com.
2021-05-25 1:08 PM
in fact both.
I try to use the FFT with my nucleo but I can't. the CMSIS site dont give a lot of information. just the command.
I can't found a simple example on use a fft on a sinus sample by the ADC.
but thank for the link, I will check
2021-05-26 11:46 AM
Hello @Seth1er,
I recommend you checking the applications on the AN4841 with the X-CUBE-DSPDEMO firmware package that demonstrates the usage of DSP including an FFT example and an FIR example to show a full integration with the STM32 families using its peripherals.
You can as well take advantage of using free ST IDE; STM32CubeIDE, by referring to the Configuring DSP libraries on STM32CubeIDE article.
Chahinez.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.