2020-02-12 5:40 AM
Hello,
currently I'm trying to use the LPUART of the MCU using the LL drivers but I encountered an annoying issue.
In short:
LPUART1_TX = PB6
LPUART1_RX = PB7
-> Tx not working, pin always low; Rx fine
LPUART1_TX = PA1
LPUART1_RX = PB7
-> Everything working as it should
More details:
For project setup and development I use the STM32CubeIDE on Linux. On the forums I found an older entry that LL drivers don't enable the LPUART so Il had to set CR1->UE to 1.
Thus I managed to get Rx to work, yet Tx is not working on PB6 of my MCU. Changing Tx to PA1 in the device configuration tool and regenerating the code is making it work; But this is not the solution I want.
According to the schematics of the Nucleo board, PB6 is not used by anything. So I don't know if this is an issue with the MCU, Software or something else.
So if someone had prior experiences with such issues, I would be glad to hear from you.
Best regards,
Thorsten F.
PS: The generated code is below. CTS is currently grounded, but I don't think this is a problem since PA1 works.
void MX_LPUART1_UART_Init(void)
{
LL_LPUART_InitTypeDef LPUART_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
/* Peripheral clock enable */
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_LPUART1);
LL_IOP_GRP1_EnableClock(LL_IOP_GRP1_PERIPH_GPIOA);
LL_IOP_GRP1_EnableClock(LL_IOP_GRP1_PERIPH_GPIOB);
/**LPUART1 GPIO Configuration
PA6 ------> LPUART1_CTS
PB6 ------> LPUART1_TX
PB7 ------> LPUART1_RX
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_6;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_4;
LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
GPIO_InitStruct.Pin = LL_GPIO_PIN_6;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_6;
LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
GPIO_InitStruct.Pin = LL_GPIO_PIN_7;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_6;
LL_GPIO_Init(GPIOB, &GPIO_InitStruct);
LPUART_InitStruct.BaudRate = 115200;
LPUART_InitStruct.DataWidth = LL_LPUART_DATAWIDTH_8B;
LPUART_InitStruct.StopBits = LL_LPUART_STOPBITS_1;
LPUART_InitStruct.Parity = LL_LPUART_PARITY_NONE;
LPUART_InitStruct.TransferDirection = LL_LPUART_DIRECTION_TX_RX;
LPUART_InitStruct.HardwareFlowControl = LL_LPUART_HWCONTROL_CTS;
LL_LPUART_Init(LPUART1, &LPUART_InitStruct);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.