2017-06-02 1:43 PM
Hello
I'm trying to use TSC of my Nucleo-32 STM32F303 by changing TouchSensing_2touchkeys project of STM32Cube_FW_F3_V1.8.0 . I want to create one touch button and I try both TSC group 3 and TSC group 6 of my board . when I use group 3 it sets ISR register to 0x03 that means max count error has occurred and when I use group 6 it set ISR register to 0x01 even when I totally disconnected the board from sampling capacitor and electrode and it doesn't react to finger presence . I change following parameters from original
TouchSensing_2touchkeys project :
sets number of channels , banks , objects and touch keys to 1 in tsl_conf.h .
remove all parameters related to second touch keys on tsl_user.c .
you could find modified project
https://drive.google.com/open?id=0B0TF8XZxvk7zbGVmZEt3dlQzQU0
.#nucleo-boards #stm32 #tsc2017-06-09 4:01 AM
Hi
Moghaddam.Hossein
,Thanks for sharing your project.
If you have other projects that you would like to share with other community members, you can do it in the dedicated space
https://community.st.com/community/share-your-activities
.-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.