2019-08-10 5:28 AM
Hi,
I am new to STM32 H7. I designed 1 board using STM32H750VBT6. But when i try to erase internal flash using keil IDE, it is showing 'Flash Timeout: Reset the target and try it again'. I have attached the scrennshot of the error.
2019-08-13 12:55 AM
I am able to erase and write the code into the flash but control is not coming to main function.
But if i try to run the same code from internal ram, it is working fine. I checked even the vector table is at the correct address.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.