2010-07-05 9:55 AM
No definition for DWT in Core_cm3.h?
2011-05-17 4:57 AM
Why would you want to access the
http://infocenter.arm.com/help/topic/com.arm.doc.ddi0337h/BIIFBHIF.html
(DWT) from code? Typically a debugger does that. If you really want to you can look at thehttp://infocenter.arm.com/help/topic/com.arm.doc.ddi0337h/BABJFFGJ.html
.2011-05-17 4:57 AM
Thank you for the link.
I want to use the cycle counter feature to measure the time for different routines. Also, I was thinking of using it for delay loops... I would think regardless of the usage, the registers would be documented...2011-05-17 4:57 AM
Hello,
It seems that you can't use cycle counter for delay loops. When you read Cortex-M3 documentation from ARM, DDI0337G, there is a register at address 0xE000EDFC named DEMCR (Debug exception and Monitor Control Register) (chapter 10.2.4). In this register, bit TRCENA (bit 24) must be set to enable use of DWT which contains cycle counter. But in chapter 10.1, documentation say that this register can't be accessed by the processor itself but only by the debugger. I made some tests and I have seen that it not possible to enable cycle counter without a debugger like Jlink in JTAG or SWD mode. Regards Eric2011-05-17 4:57 AM
I made some tests and I have seen that it not possible to enable cycle counter without a debugger like Jlink in JTAG or SWD mode.
Pretty sure that's hogwash. The cycle counter on the STM32F103RET6 within the trace unit is totally usable from a serial terminal , with no JTAG pod anywhere near the device. // From http://forums.arm.com/index.php?showtopic=13949 volatile unsigned int *DWT_CYCCNT = (volatile unsigned int *)0xE0001004; //address of the register volatile unsigned int *DWT_CONTROL = (volatile unsigned int *)0xE0001000; //address of the register volatile unsigned int *SCB_DEMCR = (volatile unsigned int *)0xE000EDFC; //address of the register *SCB_DEMCR = *SCB_DEMCR | 0x01000000; *DWT_CYCCNT = 0; // reset the counter *DWT_CONTROL = *DWT_CONTROL | 1 ; // enable the counter #define STOPWATCH_START { cyc[0] = *DWT_CYCCNT;} #define STOPWATCH_STOP { cyc[1] = *DWT_CYCCNT; cyc[1] = cyc[1] - cyc[0]; }
2011-05-17 4:57 AM
Hello,
You are right. I made a mistake in my test. I try to enable cycle counter by writing in DWT_CONTROL before writing in SCB_DEMCR. By swapping the 2 writes, cycle counter is ok even without a debugger. Thank you EricWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.