2023-12-05 9:42 PM
Hi we're using STM32L412RB controller for our development wanted to know what are preferable IDE that can be used for the software development for the purchased controller.(They've suggested us for Eclipse wanted to make sure is it okay to use eclipse if yes what are the advantages and disadvantages of that)
Also need the suitable emulator information/suggestion regarding this?
Solved! Go to Solution.
2023-12-19 12:23 AM
Hello again @Adithya_Jayaram
You have just to wire the necessary pins according to the debug mode you are using (JTAG/SWD). For that, you can refer to the RM0394 part 46.4.1 and the DS12469 for the board and the UM2910 for the STLINK-V3MINIE.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.