2016-10-08 1:46 PM
Hi,
I use STM32L073 and configure SPI port. Problem is my slave device has SPI_MISO pin as open-drain, very uncommon. Question is if I configure MCU pin as SPI_MISO can I have also pull-up function on that pin or need external? Darko2016-10-09 3:18 AM
> Question is if I configure MCU pin as SPI_MISO can I have also pull-up function on that pin
Yes. However, the internal pull-up is relatively weak - check if the resulting RC (with the parasitic C of the MISO pins and tracks) is fast enough for your bitrate. JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.