2019-09-09 1:06 PM
I am using the STM32 Nucleo F411RE, and have 5 GPIO pins set up as inputs, each set to trigger an interrupt on the rising and falling edge, configured to use the internal pull down.
However, what I am finding is that causing a level change on one of the pins is triggering an interrupt for all of them.
At first I thought it might be cross talk between the pins, but I added external pull down resistors of 10k to ground and the issue is still there.
So I'm assuming either my configuration is wrong, or my interrupt handlers are, but I don't see any issue..
#define PEDAL_CLAMP_Pin GPIO_PIN_2
#define PEDAL_CLAMP_GPIO_Port GPIOC
#define PEDAL_FORWARD_Pin GPIO_PIN_3
#define PEDAL_FORWARD_GPIO_Port GPIOC
#define PEDAL_REVERSE_Pin GPIO_PIN_6
#define PEDAL_REVERSE_GPIO_Port GPIOC
#define PEDAL_UNCLAMP_Pin GPIO_PIN_8
#define PEDAL_UNCLAMP_GPIO_Port GPIOC
#define SWITCH_PRESSURE_Pin GPIO_PIN_10
#define SWITCH_PRESSURE_GPIO_Port GPIOC
void MX_PedalSwitches_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
BaseType_t createStatus = pdFAIL; // Init to fail to be safe
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
GPIO_InitStruct.Pin = PEDAL_CLAMP_Pin|PEDAL_UNCLAMP_Pin|PEDAL_FORWARD_Pin|PEDAL_REVERSE_Pin
|SWITCH_PRESSURE_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING_FALLING;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
HAL_NVIC_SetPriority(EXTI15_10_IRQn, configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY, 0);
HAL_NVIC_SetPriority(EXTI3_IRQn, configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY, 0);
HAL_NVIC_SetPriority(EXTI2_IRQn, configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY, 0);
HAL_NVIC_SetPriority(EXTI9_5_IRQn, configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY, 0);
HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);
HAL_NVIC_EnableIRQ(EXTI3_IRQn);
HAL_NVIC_EnableIRQ(EXTI2_IRQn);
HAL_NVIC_EnableIRQ(EXTI9_5_IRQn);
createStatus = xTaskCreate(SwitchDebounceTask, "Pedal Switch task", configMINIMAL_STACK_SIZE,(void*) NULL,1, &switchTaskHandle);
configASSERT(createStatus == pdPASS);
}
void EXTI2_IRQHandler(void)
{
BaseType_t xHigherPriorityTaskWoken = pdFALSE;
uint32_t notifyValue = 0;
if(__HAL_GPIO_EXTI_GET_IT(PEDAL_CLAMP_Pin) != RESET)
{
notifyValue = 1 << PEDAL_CLAMP_PRESSED;
xTaskNotifyFromISR(switchTaskHandle, notifyValue, eSetBits, &xHigherPriorityTaskWoken);
}
__HAL_GPIO_EXTI_CLEAR_IT(PEDAL_CLAMP_Pin);
portYIELD_FROM_ISR( xHigherPriorityTaskWoken );
}
void EXTI3_IRQHandler(void)
{
BaseType_t xHigherPriorityTaskWoken = pdFALSE;
uint32_t notifyValue = 0;
if(__HAL_GPIO_EXTI_GET_IT(PEDAL_FORWARD_Pin) != RESET)
{
notifyValue = 1 << PEDAL_FORWARD_PRESSED;
xTaskNotifyFromISR(switchTaskHandle, notifyValue, eSetBits, &xHigherPriorityTaskWoken);
}
__HAL_GPIO_EXTI_CLEAR_IT(PEDAL_FORWARD_Pin);
portYIELD_FROM_ISR( xHigherPriorityTaskWoken );
}
void EXTI9_5_IRQHandler(void)
{
BaseType_t xHigherPriorityTaskWoken = pdFALSE;
uint32_t notifyValue = 0;
if(__HAL_GPIO_EXTI_GET_IT(PEDAL_REVERSE_Pin) != RESET)
{
notifyValue = 1 << PEDAL_REVERSE_PRESSED;
xTaskNotifyFromISR(switchTaskHandle, notifyValue, eSetBits, &xHigherPriorityTaskWoken);
__HAL_GPIO_EXTI_CLEAR_IT(PEDAL_REVERSE_Pin);
}
if(__HAL_GPIO_EXTI_GET_IT(PEDAL_UNCLAMP_Pin) != RESET)
{
notifyValue = 1 << PEDAL_UNCLAMP_PRESSED;
xTaskNotifyFromISR(switchTaskHandle, notifyValue, eSetBits, &xHigherPriorityTaskWoken);
__HAL_GPIO_EXTI_CLEAR_IT(PEDAL_UNCLAMP_Pin);
}
portYIELD_FROM_ISR( xHigherPriorityTaskWoken );
}
void EXTI15_10_IRQHandler(void)
{
BaseType_t xHigherPriorityTaskWoken = pdFALSE;
uint32_t notifyValue = 0;
HAL_EXTI_IRQHandler(&H_EXTI_13);
if(__HAL_GPIO_EXTI_GET_IT(SWITCH_PRESSURE_Pin) != RESET)
{
notifyValue = 1 << SWITCH_PRESSURE_PRESSED;
xTaskNotifyFromISR(switchTaskHandle, notifyValue, eSetBits, &xHigherPriorityTaskWoken);
__HAL_GPIO_EXTI_CLEAR_IT(SWITCH_PRESSURE_Pin);
}
portYIELD_FROM_ISR( xHigherPriorityTaskWoken );
}
2019-09-09 1:14 PM
Can you replicate this behaviour in a simple/minimal, non-RTOS, implementation?
2019-09-09 8:44 PM
Does it still do that, if you add clearing of interrupts before enabling them? Rather before setting priorities.
2019-09-13 6:25 AM
After clearing interrupts before setting priorities it still does it... I'm working on putting a simple example together to try it, but it may be a few days before I can get to it
2019-09-14 1:21 AM
HAL_EXTI_IRQHandler(&H_EXTI_13);If you process interrupt with your code, why to you need this?
> However, what I am finding is that causing a level change on one of the pins is triggering an interrupt for all of them.
How exactly do you determine that?
2019-09-16 7:04 AM
I'll have to look at that.. I think it was auto generated.
I have different tasks running that process each interrupt, when the interrupt occurs I send a flag to the task, which then unblocks and does something... I can see all the tasks unblocking
2019-09-19 7:23 AM
Are some of the GPIO pins only 3.3V tolerant as inputs? As I've been looking into this more I've seen some references to that, but I didn't see anything in the data sheet...I didn't realize this and have been using 5V signals.
2019-09-19 1:33 PM
I reproduced the behavior without freertos, I did everything in main... I hooked up a scope on one of the lines and there is tons of noise, with spikes over 2.5 volts.
For now I've transitioned to polling instead of using interrupts until I can sort this out more.
I added external pull down resistors without changing the behavior
2023-10-06 12:30 AM
Same problem, I tried this to debug and both ent1 and ent2 are loaded with 1 at same time
void EXTI0_IRQHandler(void)
{
/* USER CODE BEGIN EXTI0_IRQn 0 */
ent1 = 1;
/* USER CODE END EXTI0_IRQn 0 */
HAL_GPIO_EXTI_IRQHandler(IN_1_Pin);
/* USER CODE BEGIN EXTI0_IRQn 1 */
/* USER CODE END EXTI0_IRQn 1 */
}
/**
* @brief This function handles EXTI line1 interrupt.
*/
void EXTI1_IRQHandler(void)
{
/* USER CODE BEGIN EXTI1_IRQn 0 */
ent2 = 1;
/* USER CODE END EXTI1_IRQn 0 */
HAL_GPIO_EXTI_IRQHandler(IN_2_Pin);
/* USER CODE BEGIN EXTI1_IRQn 1 */
/* USER CODE END EXTI1_IRQn 1 */
}
I have 16 exti's but I only programmed 2, exti0 and exti1 to start the develop, when I trigger the first the second is triggered also and viceversa
2023-10-06 12:31 AM
I tried with irq0 for all and after that I tried with irq0 for exti0, irq1 for exti1 and so on
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.